Panel Design & Build

Side Navigation

  • Page links will be generated when this page has been added to the Link List

Our Panel Fabrication Facility outputs product that is:

  • The highest quality
  • Manufactured in the most cost effective way
  • Built to the required specification

System Build

System Build encompasses panel fabrication and testing, and the staging of the complete system (control systems panels, marshalling panels, networks, operator consoles, configuration stations, and all associated software) for integration testing, customer inspection and Factory Acceptance Testing (FAT).

Panels are a vital link between the operator interface and the field instrumentation and are an integral part of the overall control strategy. Good design is of paramount importance. Proper layout of the panel and efficient use of available space is vital in today's complex and compact processing plants. Furthermore, to allow for possible expansions, panels must be designed not only for today's needs but also with the future in mind.

Quality Design and Fabrication

Our panels are built to the highest International Standards, from design right through to construction and testing. This ensures a consistent, high quality product each and every time. The use of our extensive CAD facilities for all panel designs allows us to preview the panel layout at all stages of the design process and quickly and easily implement any changes.

To capitalize on good design we only use top quality components and the highest standards of workmanship throughout our panels. Following construction, we comprehensively test all our panels. These tests can include full systems tests (DCS, PLC, PC, SCADA, etc.) if required.