Assessment Services

Related Links

Assessment Services

Safety Assessments

Safety Assessments help you comply with current and emerging standards by providing consulting services for safety critical controls. Our solutions can help reduce lost-time accidents, improve workplace safety and improve employee morale, which will ultimately result in increased productivity.

Hazard  Risk  Arc Flash  CE Mark  Lockout/Tagout  Stop Time  Safety Circuit    

An Arc Flash Analysis helps identify issues that may lead to an arc flash or blast. An arc flash or blast can release dangerous levels of heat energy, fire, molten materials, vaporized solids that can be inhaled, flying shrapnel and trigger the rapid expansion of air, all capable of causing severe and sometimes fatal injuries. To help reduce the risk of an arc flash or blast, and the associated injuries, a Rockwell Automation Arc Flash Analysis includes:

Rockwell Automation can perform problem remediation and updates to one-line diagrams following the assessment.