Environmental

Rockwell Automation Software Environmental

Have a Question?

Related Links

Application Profiles

Case Studies

Environmental

SOFTWARE CEM®: PREDICTIVE EMISSIONS MONITORING SYSTEM

Software CEM is the first Predictive Emissions Monitoring System (PEMS). Introduced in 1992 and approved by the U.S. EPA as a PEMS, Software CEM provides real-time emissions monitoring through correlations with existing instruments-resulting in accurate, fast emissions information.

Software CEM provides a more cost-effective emissions monitoring compliance than hardware-based alternatives. Proven in more than 250 installations, Software CEM uses the powerful Pavilion8 model analytic engine and the patented sensor validation system to assure regulatory compliance with unparalleled accuracy and reliability.

Software CEM has served as the basis for PEMS requirements worldwide. Its built-in sensor validation system detects and compensates for failed or drifting sensors-resulting in higher uptime, rapid reconstruction of bad sensor values and early detection of improper unit operation. What's more, it is a fraction of the cost of hardware CEMS to install, certify and maintain.

Software CEM Benefits

Cost Effective Monitoring & Compliance

Highly Accurate and Reliable Emissions Monitoring and Reporting

Environmental and Industrial Expertise