New Rockwell Automation Power Monitors Help Companies Control and Reduce Industrial Energy Consumption
Two new models feature wireless capabilities and improved energy-data display to simplify energy-consumption tracking
MILWAUKEE, Jan. 23, 2012 — Two new Allen-Bradley power monitors from Rockwell Automation provide manufacturers with scalable, cost-effective insight into how, when and where energy is being used throughout the production process. The Allen-Bradley PowerMonitor W250 and 500 power meters offer users an opportunity to cost-effectively drive energy monitoring further into their production processes compared to previous monitoring technology.
“Many manufacturers are looking to gain deeper insight and data granularity of their industrial energy consumption,” explained Phillip Bush, power and energy management product manager, Rockwell Automation. “These two new power monitors allow our customers to drill down beneath facility or process-level monitoring to collect data from specific energy-intensive applications without significant cost and effort.”
The PowerMonitor W250 power meter offers a self-generating wireless communications platform, ideally suited for applications located in areas where hard-wired networking is cost prohibitive. The PowerMonitor 500 power meter features a large LCD display to view energy use information directly at the process being monitored without requiring any additional components.
The wireless PowerMonitor W250 power meter is capable of measuring energy consumption at multiple metering locations, including remote or confined spaces such as ceilings, conveyor belts or outdoors. Completely cable-free, the self-generating wireless network transmits energy consumption information directly to Rockwell Software RSEnergyMetrix software for reduced networking costs and easier data collection. Simplified networking for additional monitors allows for improved system modularity and flexibility.
For smaller consumption and demand-monitoring applications, the PowerMonitor 500 power meter features an on-device LCD display in a small, panel-mounted footprint. Operators can access real-time energy demand and consumption data at the machine or process level to drive employee engagement in energy-savings initiatives. It also features Modbus TCP and EtherNet/IP communication options and is fully integrated with RSEnergyMetrix software. Energy consumption data can be loaded directly to Web-based dashboards to provide a cost-effective tool for implementing and verifying energy-saving initiatives.
About Rockwell Automation
Rockwell Automation, Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs about 21,000 people serving customers in more than 80 countries.
For more information:
- PowerMonitors – http://ab.rockwellautomation.com/Energy-Monitoring/
- The Allen-Bradley PowerMonitor 500 power meter – http://www.flickr.com/photos/rockwellautomation/6717105815/
- The Allen-Bradley PowerMonitor W250 power meter – http://www.flickr.com/photos/rockwellautomation/6717103973/in/photostream/
Media contacts:
Ken Brunnbauer
Rockwell Automation
414.328.0147
kjbrunnbauer@ra.rockwell.com
Sarah Riley
Padilla Speer Beardsley Inc.
612.455.1728
sriley@padillaspeer.com
Allen-Bradley, LISTEN. THINK. SOLVE., PowerMonitor, Rockwell Software and RSEnergyMetrix are trademarks of Rockwell Automation, Inc.
Modbus is a trademark of Modicon.
EtherNet/IP is a trademark of ODVA.