New On-Machine Motor Controller from Rockwell Automation Provides Simplified Installation and Space Savings for Machine Builders
Allen-Bradley ArmorStart LT distributed motor controllers offer a compact, modular solution that puts motor control on or near the machine, ideal for light-industrial, material-handling applications
MILWAUKEE, Jan. 12, 2012 — Machine builders can now offer customers a compact distributed motor controller that easily installs on the machine without an enclosure, and quickly connects to the enterprise network, thanks to the new family of Allen-Bradley ArmorStart LT distributed motor controllers from Rockwell Automation.
ArmorStart LT distributed motor controllers are ideal for coordinating conveyor motor systems used in material handling and packaging applications and other types of warehouse distribution systems. The new family of distributed motor controllers provides the advantages of On-Machine architecture – a pre-engineered system that helps simplify wiring, speeds up commissioning time and reduces the need for extra cabinet space.
ArmorStart LT with EtherNet/IP connectivity improves the exchange of critical information about machine performance and component health, while allowing operators to access parameters, status and diagnostics, regardless of location.
“Machine builders need to provide motor control solutions that accommodate customers’ budgets and existing network architecture,” said Paul Gieschen, market development director, Rockwell Automation.
“The new ArmorStart LT distributed motor controllers provide enhanced motor control at a lower price point and smaller package than other On-Machine motor control products on the market.”
ArmorStart LT is ideal in size and weight for most general material handling applications, making it easier to integrate on or near the conveyor or machine.
Installation also is simplified by the distributed motor controllers’ dual-port EtherNet/IP switch technology, which supports device-level ring (DLR) network topology. DLR-based networks reduce configuration time and costs by minimizing the number of managed switches and reducing cabling needs. Users can create a single DLR network that connects all components at the device level locally. Information can be seamlessly communicated in real time to various levels of an organization, without requiring additional complexity. Getting real time information at the right time and at the right levels of the manufacturing environment can enhance the agility of a business.
The distributed motor controllers include an add-on profile for Rockwell Software RSLogix 5000, the software used to program Allen-Bradley CompactLogix and Allen-Bradley ControlLogix programmable controllers from Rockwell Automation. The add-on profile’s automatic, predefined tag names provide manufacturers with a common language that can help improve consistency, and programming speed and efficiency.
The ArmorStart LT distributed motor controllers support a transparent clock to synchronize motor devices on an EtherNet/IP architecture, accommodating for delays introduced by other devices on the network. To help enhance safety, the devices contain a standard, local disconnect feature that allows operators to turn off the motor and perform lockout tagout procedures during maintenance. They also are group-motor listed so multiple units can be grouped under one branch circuit protection device.
Rockwell Automation, Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs about 21,000 people serving customers in more than 80 countries.
For more information:
- Allen-Bradley ArmorStart LT Distributed Motor Controllers product information:
http://ab.rockwellautomation.com/motor-control/armorstart-distributed-motor-controller
- Allen-Bradley ArmorStart LT Distributed Motor Controller image: http://www.flickr.com/photos/rockwellautomation/6643085231/in/photostream/
- Allen-Bradley ArmorStart LT Distributed Motor Controller image: http://www.flickr.com/photos/rockwellautomation/6643084405/in/photostream/
Media contacts:
Sarah Larson
Rockwell Automation
414.382.5910
selarson@ra.rockwell.com
Mick Forgey
Padilla Speer Beardsley Inc.
612.455.1789
mforgey@padillaspeer.com
Allen-Bradley, ArmorStart, ControlLogix, CompactLogix, LISTEN. THINK. SOLVE. and On-Machine, Rockwell Software and RSLogix are trademarks of Rockwell Automation, Inc.
EtherNet/IP is a trademark of ODVA.
###