Investor Relations
Board Committee Description
Board Composition and Governance Committee
The members of the Board Composition and Governance Committee are William T. McCormick, Jr. (Chairman), Verne G. Istock, David B. Speer, and Joseph F. Toot, Jr. The principal functions of the Board Composition and Governance Committee are to consider and recommend to the Board qualified candidates for election as directors of the Corporation and to prepare and submit to the Board the Committee's selection criteria for director nominees. The Committee annually assesses and reports to the Board on the performance of the Board of Directors as a whole and of the individual directors. The Committee also recommends to the Board the members of the Committees of the Board and the terms of our Guidelines on Corporate Governance. All members of the Committee are independent directors as defined by the NYSE. The Committee met five times during the 2007 fiscal year.
The Committee will consider candidates for director recommended by shareowners. Shareowners wishing to recommend director candidates can do so by writing to the Secretary of the Corporation at 1201 S. 2nd Street, Milwaukee, Wisconsin 53204. The recommendation must include the candidate's name, biographical data and qualifications and any other information required by the SEC to be included in a proxy statement with respect to a director nominee. Any such recommendation must be accompanied by a written statement from the candidate indicating his or her willingness to serve if nominated and elected. The recommending shareowner also must provide evidence of being a shareowner of record of our Common Stock at that time.
The Committee, the Chairman and Chief Executive Officer or other members of the Board may identify a need to add new members to the Board or fill a vacancy on the Board. In that case, the Committee will initiate a search for qualified director candidates, seeking input from senior management and Board members, and to the extent it deems it appropriate, outside search firms. The Committee will evaluate qualified candidates and then make its recommendation to the Board for its consideration and approval.
In making its recommendations to the Board with respect to director candidates, the Committee considers various criteria set forth in our Board Membership Criteria (see Exhibit A to the Committee's Charter), including experience, professional background, specialized expertise and concern for the best interests of shareowners as a whole. In addition, directors must be of the highest character and integrity, be free of conflicts of interest with the Corporation, and have sufficient time available to devote to the affairs of the Corporation. The Committee from time to time reviews with the Board our Board Membership Criteria in the context of the current composition of the Board and our circumstances.
The Committee will evaluate properly submitted shareowner recommendations under substantially the same criteria and in substantially the same manner as other potential candidates.
In addition to recommending director candidates to the Committee, shareowners may also nominate candidates for election to the Board at annual shareowner meetings by following the procedures set forth in our By-Laws.