Press Releases

Evolution of Design Environment From Rockwell Automation Sets Foundation for Future of Integrated Architecture System

Share This Studio 5000 unified engineering and design environment paves the way to one standard software for all of your automation control needs

PHILADELPHIA, Nov. 7, 2012 — Rockwell Software Studio 5000 unified engineering and design environment, releasing later this month from Rockwell Automation, provides a framework for engineering collaboration. It sets the foundation for design tools that allow engineers to enter configuration and programming information only once, and then leverage it across their entire control system architecture from design to operation to maintenance.

“The Studio 5000 environment will bring the Rockwell Automation Integrated Architecture system to the next level, building on the superior usability of Rockwell Software RSLogix 5000 software, further improving the user experience, and the design and productivity of automation systems,” said Kevin Zaba, vice president and general manager, Control and Visualization Business, Rockwell Automation. “Optimally integrated hardware and software means users can define data once and easily use it across the Integrated Architecture system. The data and tag structures are natively recognized and automatically picked up by the other system components, improving development efficiency and reducing programming errors. A unified engineering and design environment also communicates and performs at higher speeds. For customers, the result is improved productivity, shorter design cycles and a faster time-to-market.”

The debut of Studio 5000 software includes the Logix Designer application for programming and configuration of Allen-Bradley ControlLogix 5570 and CompactLogix 5370 programmable automation

controllers. Later versions will provide applications for other engineering tasks, such as HMI development, library management for reusable components, information integration and more.

Maintaining the familiar, user-friendly workflows and interfaces from the RSLogix 5000 design and configuration software, the new Studio 5000 environment creates an optimal level of integration within the Integrated Architecture system. Optimal integration is accomplished by embedding features such as program comments and descriptions, and a new alarm log, directly in the controller.

The new environment taps additional memory storage capacity in the latest generation of Logix controllers so program comments, for example, that describe the functionality of each line of code, can be maintained directly in the controller without reducing available user memory. Now, a complete project can be stored in the controller, with comments correlated for multiple users, reducing time and effort related to maintenance and troubleshooting.

Additionally, the Studio 5000 environment creates a controller-based (versus HMI-based) alarm log. Storing this information in the controller means alarm data will not be lost if there is a communication or network failure between the HMI and the controller. Additionally, support for the ISA 18.2 state model allows for simpler creation of alarming systems that align with this widely accepted recommendation. The Studio 5000 unified engineering and design environment is available globally under the same catalog number as RSLogix 5000 software.

About Rockwell Automation
Rockwell Automation, Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs over 22,000 people serving customers in more than 80 countries.

For more information:

Media contacts:
Gigi O’Neill
Rockwell Automation
440.646.3192
ggoneill@ra.rockwell.com

Sarah Kalhorn
Padilla Speer Beardsley Inc.
612.455.1791
skalhorn@padillaspeer.com

Allen-Bradley, CompactLogix, ControlLogix, Integrated Architecture, LISTEN. THINK. SOLVE., Rockwell Software, RSLogix and Studio 5000 are trademarks of Rockwell Automation, Inc.

# # #