Entitlement Online activation
Complete the Runtime entitlement online activation if the Runtime device is connected to the Internet.
NOTE:
The entitlement serial number XXXXX-XXXXX-XXXXX-XXXXX-XXXXX is used in the following instructions as a placeholder.
- To allow for entitlement activation, launch the FTOptixEntitlementCli.sh, a self-installing shell script.NOTE: Only a superuser can install the FactoryTalk Optix Entitlement Manager CLI program for entitlement activation.
- In a terminal, entersudo ./FTOptixEntitlementCli --onlineActivate --entitlementKey XXXXX-XXXXX-XXXXX-XXXXX-XXXXX.
- Entersudo ./FTOptixEntitlementCli --showInstalledEntitlementto view entitlement details.
Provide Feedback