Create an alarm

Create an alarm that indicates conveyor chassis malfunctions.
  1. Create an input variable:
    1. In
      Project view
      , right-click
      Model
      and select
      New
      Variable
      .
    2. Hover-over the variable, select
      Edit
      , and enter
      ConveyorChassisMalfunctionAlarmVariable
      :
    3. Select
      ConveyorChassisMalfunctionAlarmVariable
      , and in
      Properties
      , select
      Int32
      and select
      Boolean
      .
  2. Create the alarm:
    1. In
      Project view
      , right-click
      Alarms
      and select
      New
      Digital alarm
      .
    2. Hover-over the alarm, select
      Edit
      , and enter
      ConveyorChassisMalfunction
      .
  3. Configure the alarm:
    1. In
      Properties
      , create a dynamic link between
      Input variable
      and
      ProjectName
      Model
      ConveyorChassisMalfunctionAlarmVariable
      .
      For more information about dynamic links, see Create dynamic links.
    2. Set
      Message
      to
      Conveyor chassis malfunctioned
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.