Protection against domain change

Stratix 4300 Remote Access
routers are compliant with the security standards of
FactoryTalk Remote Access Manager
to protect both the installer and the end user against unwanted and non-authorized domain change attempts.
This means that the device registration domain cannot be changed, since the registration information is stored on the server once the device is registered. For this reason, the device is registered to the domain until it will be completely removed from the same.
NOTE: See Remove and move devices for further information on this subject.
In case of non-authorized domain change attempt, a security block triggers, preventing the router from being registered to a domain and the
Device Registration
Tool will return an error message.

Restore Operation

To restore the router operation after a security block, contact the Technical Support Team.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.