Rehost an entitlement on Ubuntu 22.04 devices

Rehost an entitlement for use on another device by using the command below:
NOTE: The entitlement serial number XXXXX-XXXXX-XXXXX-XXXXX-XXXXX appears in this procedureas a placeholder.
  1. In a terminal, enter
    sudo ./FTOptixEntitlementCli --rehost --entitlementKey XXXXX-XXXXX-XXXXX-XXXXX-XXXXX
    .
    The message
    Entitlement rehosted successfully
    appears.
  2. (optional) To view updated entitlements, from the FactoryTalk landing page, select
    Entitlements
    Organization Entitlements
    .
    NOTE: You must be an admin or owner to view entitlement status.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.