Develop an interface for switching locales

Create a localized label and two buttons that change the interface language.
Application example - English locale
Application example - Polish locale
NOTE:
Download a sample project:
SwitchLocales.zip
Prerequisites
  1. To develop the project
  2. Arrange the interface elements.
  3. Save the project.
Application design example
Select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.