Develop a solution for importing UI

Use OPC UA communication to import the UI from another project and display the values of selected variables.
Application example (server and client)
TIP:
Download a sample project:
ImportUI.zip
Prerequisites
TIP: The Client project imports data from the Server project.
Application design example (server and client)
Select
Run
to run server and client projects using the client emulator to test your project. To run the projects on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.