Create an alarm

Create an exclusive level alarm that warns about exceeded temperature.
  1. In
    Project view
    , right-click
    Alarms
    and select
    New
    Exclusive level alarm
    .
  2. In
    Properties
    , set
    High limit
    to
    60
    .
  3. Set
    Auto confirm
    to
    True
  4. Set
    Message
    to
    Maximum temperature exceeded
  5. Create a dynamic link between
    Input variable
    and
    ProjectName
    Model
    Temperature
    .
    For more information about dynamic links, see Create dynamic links.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.