Router registration, connection and configuration

The router system software is designed to require just a few mandatory settings in order to reduce manual configuration as much as possible. In fact, the VPN and Ethernet interfaces configuration is already defined in the factory default settings. Nevertheless, you are required to configure specific manual settings, such as: network interfaces IP addresses, connection mode, and domain registration.
Once configured, the router connects to the Server Infrastructure and can be detected by
FactoryTalk Remote Access Manager
.
Prior to getting started with the router configuration, you will have to register it.
NOTE: See FactoryTalk Remote Access Manager Tools to learn your Tool of reference for router registration. Then, follow the related procedure below.

Device registration

You can access the
Device registration
Tool as follows:
  1. Access the FactoryTalk Remote Access Manager and select
    Explorer
    Domain view
    .
  2. Click on the
    circled plus
    icon next to a folder: a context menu will appear.
  3. Select
    Add device
    Add device locally
    .
    NOTE:
    The
    Add Device Locally
    parameter refers to routers registration only.
    NOTE: dialog window appears asking for permission to open the Tool. Prior to confirming, flag the
    Always allow
    checkbox to prevent this message from prompting again during this session. If you use a different computer or a different browser, this message will prompt again.
  4. Enter the router credentials in the Tool.
  5. Select
    Next
    .
  6. The
    Routers found
    list displays the MAC addresses of the routers in your domain that have a password matching the one specified.
    NOTE:
    When setting up Stratix 4300 Remote Access routers, the username of the router is always
    admin
    and cannot be changed. The default password is
    admin
    and shall be changed during the initial configuration.
    You can change the router password anytime through the router System Manager, in the
    Users
    section. Reboot your router upon any password change.
    Choose a password that contains:
    • At least one uppercase character
    • At least one lowercase character
    • At least one numeric character
    • At least one symbol
  7. Select a router MAC address from the list and click
    Register
    to open the configuration pages for that router.
    NOTE: You might be required to authenticate to the
    Device Registration
    Tool prior continuing with the router registration.
  8. The newly connected router appears below the other devices listed in the left pane of
    Explorer
    Domain view
    .

Device discovery

You can access the
Device discovery
Tool as follows:
  1. Access the
    FactoryTalk Remote Access Manager
    and select
    Tools
    Device setup
    .
  2. A dialog box appears. Choose the second choice.
    NOTE: dialog window appears asking for permission to open the Tool. Prior to confirming, flag the
    Always allow
    checkbox to prevent this message from prompting again during this session. If you use a different computer or a different browser, this message will prompt again.
  3. A discovery window appears. Click on
    Discover
    .
  4. The
    Discovered devices
    list displays the devices in your network.
  5. Select the device that you wish to configure.
    NOTE:
    Configurable
    devices are still to be initialized on the device System Manager, while
    Configured
    devices are already initialized on the device System Manager and the device credentials can be found there.

Router connection and configuration

A router can be configured through its System Manager.
  • Access
    FactoryTalk Remote Access Manager
    and
    Explorer
    Domain view
    .
  • Enable the online toggle switch and in the
    Domain view
    left pane select the online router that you wish to configure.
  • Select the
    VPN
    button.
  • The
    Interactive Access
    Tool opens and a VPN connection is established.
  • Enter the router LAN IP address that you find on the right pane of the
    Interactive Access
    screen into a browser to access the router System Manager. You will be prompted to enter username and password.
NOTE: See the System Manager documentation supplied with the device for detailed instructions.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.