Configure presentation engines
Add a native presentation engine or a web presentation engine to your project.
TIP:
Each project can contain a single native presentation engine and a single web presentation engine. If your project runs on the Embedded Edge Compute Module (1756-CMEE1Y1), add a web presentation engine and delete the native presentation engine.
- InProject view, right-click a window object and selectNew.
- Select one of these presentation engines:
- Native presentation engine. Create a native presentation engine when you are going to runFactoryTalk Optixas an application on the local device. This mode is generally used by a local user logged onto the device.
- . Create a web presentation engine when you are going to runFactoryTalk Optixas a service on the runtime device or as an application to interact with the system using a web client.FactoryTalk Optixas a service automatically runs the deployed application with or without a user interface. This mode is generally used when there is no local operator on the runtime device.
- With the presentation engine selected, inProperties, edit any properties that require modification for the presentation engine.
- To delete a presentation engine, right-click a presentation engine and selectDelete.
Provide Feedback