Develop a localized event logger

Create an even logger that displays the interface in the language of a currently logged-in user.
Application example - English
Application example - Italian
NOTE:
Download a sample project:
LocalizedEventLogger.zip
Prerequisites
Application design example
Select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.