Create a confirmation dialog widget

Add a preconfigured confirmation dialog widget from the template libraries.
  1. From the toolbar, select
    Template Libraries
    .
  2. In
    Libraries
    , search for
    Confirmation Dialog
    .
  3. Under
    Components
    , drag
    Confirmation Dialog
    into
    UI
    in
    Project view
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.