FactoryTalk Remote Access Manager Authentication
Access FactoryTalk Remote Access Manager as follows:
- Once you have created yourMyRockwellAutomationaccount, sign in to the FactorytalkHub.com webpage and authenticate by entering your MyRockwellAutomation account credentials.NOTE: See Create an organization and a domain to learn how to create a MyRockwellAutomation account.
- Select the FactoryTalk Remote Access tile, and another authentication is required.
- In the authentication window, enter the code sent to the mobile phone that you associated to this 2-factor authentication during the registration of yourMyRockwellAutomationaccount and access the application.NOTE: See Two-Factor authentication for further information on this subject.
Provide Feedback