Sizing example
The following example shows you how to access and use the sizing tool within
FactoryTalk® Hub®
. You must be logged in to be able to access the tool. As you complete each step, the tool shows you the recommended runtime package based on your selections.
NOTE:
Before you complete the steps in this section, you must first be part of an organization and have multifactor authentication configured.
- SelectFactoryTalk® Optix™from the list of available applications.
- Select Runtime Sizing from the top navigation bar.
- Follow the wizard to select the features your application needs.
For example, if you select these features:
Wizard Category | Example Selection |
Select presentation | Web HMI Client |
Select features |
|
Controller connections | Rockwell EtherNet/IP
|
Select interoperability |
|
You see these recommended runtime packages:
Select the package you want to see the associated catalog number for purchase via the Commerce Portal.
Provide Feedback