New Brochure Highlights Precision Positioning Solutions for Flat Panel Display Equipment
Shirley, New York (May 2003) - Anorad, the precision motion division of Rockwell Automation, has published a new brochure entitled 'Precision Motion Systems for Flat Panel Display Processing'. The document showcases many of the high precision positioning products Anorad offers to satisfy the unique requirements of the burgeoning flat panel display (FPD) industry. Multiple system configurations are presented which can handle substrate sizes from Gen 3 up to the latest Gen 7 specifications. The informative brochure highlights several of Anorad's latest products that can provide over 2 meter XY travels and deliver submicron repeatability while meeting stringent cleanroom or vacuum compatibility requirements. These valuable systems are used in a diverse array of FPD processing applications ranging from manufacture, inspection, and repair to assembly and substrate transport. Anorad's precision motion systems are used to produce a variety of FPDs including thin film transistor liquid crystal displays (TFT-LCDs) as well as drop-on-demand (DoD) inkjet processing for electroluminescent (EL) display technologies. The broad capabilities of Anorad's precision motion platforms combined with over a half-million industrial automation products available from Rockwell Automation provides virtually limitless possibilities for designers of FPD process equipment.